Displaying Information from a Function or Program
A running function or program does not display intermediate calculated results unless you include a command to display them. This is an important difference between performing a calculation on the entry line and performing it in a function or program.
The following calculations, for example, do not display a result in a function or program (although they do from the entry line).
Displaying Information in the History
You can use the Disp command in a program or function to display information, including intermediate results, in the history.
Displaying Information in a Dialog Box
You can use the Text command to pause a running program and display information in a dialog box. The user clicks OK to continue or clicks Cancel to stop the program.
You cannot use the Text command in a function.
Note: Displaying a result with Disp or Text does not store that result. If you expect to refer later to a result, store it to a global variable.